AXIS#.VL.ARZQ1 TO AXIS#.VL.ARZQ4

Description

AXIS#.VL.ARZQ1 sets the Q (quality factor) of the zero (numerator) of AR filter 1. This value is QZ in the approximate transfer function of the filter:

AR1(s) = [s²/(2πFZ)²+s/(QZ2πFZ) + 1]/ [s²/(2πFP)² +s/(QP2πFP) + 1]

 

The following block diagram describes the AR filter function; note that AR1 and AR2 are in the forward path, while AR3 and AR4 are applied to feedback:

AR1, AR2, AR3 and AR4 are used in velocity and position mode, but are disabled in torqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist mode.

Discrete time transfer function (applies to all AR filters)

The velocity loop compensation is actually implemented as a digital discrete time system function on the DSP. The continuous time transfer function is converted to the discrete time domain by a backward Euler mapping:

s ≈ (1-z-1)/t, where t = 62.5 µs.

The poles are prewarped to FP and the zeros are prewarped to FZ.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0.1 to 5

Default Value

AXIS#.VL.ARZQ1: 0.707

VLARZQ2 to VLARZQ4: 0.5

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.VL.ARZQ1 0x5011 0x1C UDINT 1000:1 - RW False
AXIS1.VL.ARZQ2 0x5011 0x1D UDINT 1000:1 - RW False
AXIS1.VL.ARZQ3 0x5011 0x1E UDINT 1000:1 - RW False
AXIS1.VL.ARZQ4 0x5011 0x1F UDINT 1000:1 - RW False
AXIS2.VL.ARZQ1 0x5111 0x1C UDINT 1000:1 - RW False